AXIS#.IL.KVFF
Description
This parameter sets the gain for the velocity loop feedforward. It is used when you want to add a pure torque component scaled by the velocity command.
Resulting Torque Feedforward = AXIS#.VL.CMD * AXIS#.IL.KVFF
This parameter is only used in velocity and position mode (AXIS#.OPMODE = 1 and 2).
Versions
Action | Version | Notes |
---|---|---|
Implemented | 02-00-00-000 |
General Information
Type |
Read/Write |
Units |
mArms / (rad/s) |
Range |
0 to 1000 |
Default Value |
0 |
Data Type |
Float |
See Also |
|
Stored in Non-Volatile Memory |
Yes |
Variants Supported
All variants are supported.
Fieldbus Information
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
PDO Mappable |
---|---|---|---|---|---|---|---|
AXIS1.IL.KVFF |
500ah |
0eh |
Signed32 |
- |
1000:1 |
Read/Write |
No |
AXIS2.IL.KVFF |
510ah |
0eh |
Signed32 |
- |
1000:1 |
Read/Write |
No |
Name |
ID |
Hex |
Data Type |
Access |
Units |
---|---|---|---|---|---|
AXIS1.IL.KVFF |
5812 |
16B4 |
Signed32 |
Read/Write |
- |
AXIS2.IL.KVFF |
71348 |
116B |
Signed32 |
Read/Write |
- |
Parameter |
PNU |
Data Type |
Access |
Units |
---|---|---|---|---|
AXIS#.IL.KVFF |
5812 |
Float |
Read/Write |
- |